How can we help you today?

Setup the ATV340 Drives Ethernet IP address using the optional remote keypad display.

Issue:

ATV340 programming setting up the Ethernet IP address using optional HMI.

Product Line:

ATV340 with optional keypad VW3A1113 or VW3A1111.

Environment:

All

Cause:

Programming setup Ethernet IP address

Resolution:

This programming example is if you use one of the optional keypad to program your drive.

[Communication] -[Comm parameters]- [Embd Eth Config]

-[Embd Eth Config] EtE- Menu

PAn= Add a Device name

iNOO= IP mode set to NAnu or Fixed

iCO= IP Address (IC01, IC02, IC03, IC04).

iNO= Subnet mask (IM01, IM02, IM03, IM04).

iGO= Gateway address (IG01, IG02, IG03, IG04).

After setting up your IP address and subnet address etc you will need to power cycle the drive.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center