Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to debug the Time Stamped Events with OFS test client ?
Issue
How to debug the Time Stamped Events with OFS test client ?

Product line Envirovment
OPC Factory Server

Environment
Windows 10 64 bits ,Windows Server 2019 64 bits

Resolution
Enter the property of ofsclient shortcut ,add the full path of Time Stamped Events log file .
For example , -l C:\LOG\1.TXT  is the log file path with predefined format .


"C:\Program Files (x86)\Schneider Electric\OFS\Samples\OFSClient\ofsclient.exe" -l C:\LOG\1.TXT
User may need to create this txt file in the same folder.
image.png

Start the OFSclient and add the group named with ##TSEventsGroup## , add the Time Stamped variables in this group ,the stamped events will be recorded in this log .

image.png