Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to run safety task automatically after power cycle in M580 safety CPU ?
Issue
How to run safety task automatically after power cycle in M580 safety CPU ?

Product line Envirovment
Control Expert, Unity Pro, Modicon M580 safety

Environment
Windows 10 64 bits ,Windows Server 2019 64 bits

Resolution
A warm start causes each process task – including the (MAST, FAST, AUX0, AUX1) tasks – to re-enter its operating state as of the time of the power interruption. By contrast, a warm start causes the SAFE task to enter the STOP state, unless Automatic start in RUN is selected.

snap1.JPG