Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Could you please confirm PowerLogic P3 can transfer RTD to 4-20mA output?

Issue:
Possibility of PowerLogic P3 (Advanced and standard) can transfer RTD to 4-20mA output

Product Line:
PowerLogic P3

Resolution:
PowerLogic P3 accessory external I/O can be used to transfer RTD to 4-20mA output.