Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to set the engine exerciser for a 165 Series ATS?
Answer:

1. The Automatic Generator Exerciser automatically exercises the generator for 20 minutes once every 14 days.

2. Press and release the Automatic Generator Exerciser button. After about 8 seconds the exerciser light flashes 14 times to indicate that the exerciser has been set. The number of flashes indicates the number of days until the next exercise period (at approximately the same time the button was pressed).

Group 3 Auto Exer.jpg
For further information, please refer to operator's manual 381333-163 or contact 1-800-800-2726 then dial 3 for Technical Support.