Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to identify the error codes for a 165 group 3 controller?
  • Both TRANSFER SWITCH position lights are flashing (this indicates an error condition).
165 Controller.jpg
  • Count the number of times the Automatic Generator Exerciser light flashes (repeats after a pause). This number is the error code.
165 Controller Auto Engine Exercier Light.jpg
  • Error codes:
2 light flashes - Generator failed to start.  See Problems 3 and 4.
3 light flashes - Generator failed after starting. See generator manual.
4 light flashes- Generator over frequency. See generator manual.
5 light flashes - Transfer Switch did not transfer the load to the generator. (Service required)
6 light flashes - Transfer Switch did not transfer the load to the utility. (Service required)
7 light flashes - Controller error (Service required)
  • To clear the error code, press and release the Push to Test button.
NOTE: These lights will flash only when controller power is available from either of the two power sources.

For further information, please refer to page 8 of operator's manual 381333-163 or contact 1-800-800-2726 then dial 3 for Technical Support.