Issue:
How to link variables from Ecostruxure Control Expert to Ecostruxure Operator Terminal Expert 3.2 SP2?
Product Line:
Ecostruxure Control Expert, Ecostruxure Operator Terminal Expert 3.2 SP2
Resolution:
You need to import the variables using the Symbol Link tool in EOTE, as shown below:
1.- Click on Symbol Link under Variables.
2.-Then click on +Symbol above.
3.-Specify your format file .XVM and click on Import.
4.- Browse your .XVM file and click Open.
It is important that there are caveats:
1.- There's no way to "Update" the Link. They have to be deleted and re-Link if changes are made.
2.-If you delete the Link, you lose all your Variables, Logging and Alarms from that old session.
3.- There is no way to pick and choose a subset of Variables to import - which means EVERYTHING gets imported - this could be 100,000 variables... Then you have to delete the variables you don't want ONE BY ONE.
Released for: Schneider Electric Egypt and North East Africa