Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to conduct a generator test without load transfer for a 165 Series ATS?
During the test, the generator cranks and starts, and the GENERATOR light comes on (if it is acceptable). After running for 20minutes it stops. Throughout the test, the load remains connected to the utility (the automatic transfer switch does not transfer the load to the generator).

165 Control Panel Test Button.jpg

1. Press and release (do not hold) the Push to Test button. The generator cranks and starts and the GENERATOR acceptable light comes on and stays on.

2. The generator runs for 20 minutes. The automatic transfer switch does not transfer the load to the generator. The TRANSFER SWITCH on the utility (preferred source) light stays on.

3. To bypass the time delay or cancel the test, press and release the Push to Test button again.

4. The generator stops and the GENERATOR acceptable light goes off.

For further information, you may contact Technical Support at 1-800-800-2726 then dial 3 or send an email to technicalsupport@ascopower.com.