Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a BMXCPS4002S and BMXCPS4022S redundant power supplies be used together in a redundant rack?
Different redundant power supply models are allowed in the same redundant rack as shown below.  They do not have to be of the same model number.

In this example, a BMXCPS4022S (24-48 VDC input) and a BMXCPS4002S (100-240 VAC input) are installed.
It is normal to have two different voltage sources powering a rack.
Image1


Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: