How can we help you today?

Is it possible to monitor Altivar, Altivar Process and Altivar Machine Drives for Motor Amp draw via Modbus RTU

Issue:

Can you monitor the motor Current using an Altivar ATV340 and Modbus RTU?

Product Line:

Altivar, Altivar 340 and Altivar Process Drive

Environment:

All models Altivar 340, ATV340

Resolution:

Yes, you would monitor Logic Address 3204 [LCr] Load Current via Modbus RTU

Schneider Electric Egypt and North East Africa