Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is it okay not to use the neutral provided in the transfer switch?
Answer:

If the application does not require a neutral, the answer is YES, it is okay not to use / utilize the neutral conductor provided / available in the transfer switch.

ASCO transfer switches will operate and switch between acceptable power sources even without utilizing the provided neutral conductor.  The microprocessor used on the transfer switches monitors the line voltage between the phases only.

Power Sensing Circuits