Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the ATV320 be used for Conical brake motors

Issue:
Can the ATV320 be used for Conical brake motors

Product Line:
Altivar 320, Altivar 340, Altivar 930

Environment:
All model numbers, all serial numbers

Cause:
Conical Rotor, Tapered Rotor motor

Resolution:

Yes the ATV320, ATV340, ATV930 can be used to control Conical Motor - Tapered Rotor motor

Set boA to “Static”
Set boo to -80% (minus 80%)
Set FAb to 3Hz

Boo will directly influence the fluxing current. With a negative current boost you will decrease the fluxing current and it will be enough to engage the rotor to the stator.

See attachment

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)



Schneider Electric Egypt and North East Africa

Attachment(s)
ATV320 Boost Activation.jpg [123.06 KB]