Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Can I use a 3-phase transfer switch on a 1-phase system?
Answer: YES.  3-phase transfer switches come with a microprocessor controller that can be set / programmed for 1-phase sensing.

Change the dipswitch settings from 3-phase to 1-phase and connect power cables on phases A and C.

Phase Configuration Dipswitches
Location of Dipswitches