Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is meant by " Classification of earthing switches for short-circuit making" ?
Issue:
Understanding what is meant by electrical endurance of an earthing switch and its classifications

Environment:
MV equipment
SM6 RMU

Resolution:
According to IEC62271-102; the electrical endurance of an earthing switch is the short-circuit making capability of earthing switches to perform a defined number of short circuit making operations, without major maintenance. This shall correspond to one of the classes given in Table 1.

screenshot from IEC62771-102

Schneider Electric Egypt and North East Africa