Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to do a Functional Test after installing the Series 185 automatic transfer switch?
After installing the Series 185 automatic transfer switch (ATS) perform the following three-part functional test.

1 - MANUAL OPERATION
  • A handle is provided on the transfer switch for maintenance purposes only. Manual operation of the transfer switch should be checked before it is energized.
WARNING! Do not manually operate the transfer switch until both power sources are disconnected: open both circuit breakers.
1. Turn OFF both the utility and generator circuit breakers feeding the ATS. Verify that ALL POWER IS OFF!
2. For 100–230 A - Grasp the maintenance handle and turn it quickly with your thumb and fingers to manually operate the transfer switch.

For 260 - 400 A - Insert the maintenance handle into the hole in the shaft, left side of the operator. Move the handle as shown to manually operate the transfer switch.

3. The switch should operate smoothly without binding. If it does not, check for shipping damage or construction debris.
4. After checking the manual operation, use the handle again to return the transfer switch to the utility source position.
100-230A
The letter P (utility) on the round weight is facing you.

Maintenance Handle 100-230A

260-400A
The letter N (utility) on the round weight is facing you. Remove the maintenance handle and store it on the transfer switch in the place provided.

Maintenance Handle 260-400 A

NOTICE: 260–400 A - Remove the maintenance handle before proceeding!

2 - VOLTAGE CHECKS

  • The ATS is rated for 220–240 V ac 60 or 50 Hz. Verify that both the utility and generator sources are 220–240 V ac 60 or 50 Hz.
3 - ELECTRICAL OPERATION
  • This procedure checks the electrical operation of the ATS.
1. Install the enclosure cover and tighten the screws
2. Verify that the generator battery is connected and that the generator’s starting controls are set for automatic.
3. Turn on both the utility and generator circuit breakers.
4. Verify that the Utility Acceptable and Load on Utility lights are on.
5. This step will start the generator. Press and hold the Transfer Test button until the Generator Acceptable light comes on and stays on. Then release the button.
6. After the Generator Acceptable light comes on, the ATS transfers the load from the utility to the generator (after approx. 10-second delay). The Load on Generator light comes on.
7. The ATS stays connected to the generator for 5 minutes (approx.). The utility must be acceptable for 5 minutes continuously. Then the load is transferred back to the utility. To bypass time delay, press the Bypass Time Delay button.
8. After load retransfer to utility, the generator runs 2 minutes (without load), then shuts down. The Generator Acceptable light goes off indicating that the generator is off.

This completes the Functional Test.
Supporting Document:
ASCO SERIES 185 Automatic Transfer Switches Operator’s Manual

If unsure, please contact Technical Support @ 1-800-800-2726 and press 3 or send an email to technicalsupport@ascopower.com