Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Where do I connect the power cables on an ASCO 185 Series Transfer Switch?

Wiring and Installation of the ASCO Series 185 automatic transfer switch (ATS) must be performed by a licensed electrician.

Refer to the ATS wiring diagram.

DANGER! ELECTROCUTION HAZARD: Turn off utility power and turn off the generator to prevent electrocution when wiring the transfer switch.

  • Preferred Source/Utility Source - connect power cables to Terminals L1 & L5 of the ATS
  • Alternate Source/Emergency Source - connect power cables to Terminals L2 & L6 of the ATS
  • Load - connect power cables to Terminals L3 & L7 of the ATS

Wiring 185

185 ATS


You can also download and view the wiring diagram on below link:

ASCO SERIES 185 Power Transfer Switches Product Wiring


If unsure, please contact Technical Support @ 1-800-800-2726 and press 3 or send an email to technicalsupport@ascopower.com