Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What conditional (Digital) inputs are available with EVlink Pro AC ?

Article available in these languages: Czech

There are three Digital Inputs:
Thanks to eSetup you can set them.

Delayed Charge Input (E3/E4).
Temporary power limitation (E1/E2).
Vehicle detection (E5/E6).

Note: There is no need to use an external power supply. Thanks to eSetup we are able to set active states at open or closed contacts.

eSetup