Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is a Service Entrance-rated transfer switch?
A service entrance-rated transfer switch is a transfer switch that contains an integrated disconnecting device and meets the grounding and bonding requirements of the National Electrical Code for service entrance use.

The salient features of an ASCO service entrance-rated transfer switch are (1) an integrated circuit breaker provided on the Normal side of the ATS, (2) a bonding jumper between the neutral and ground, and (3) a neutral disconnect link.

A typical outline drawing for a service entrance-rated J-Frame and the corresponding one-line diagrams are shown below as an example.


Service Entrance

Service entrance-rated units are available in the ASCO Series 185 , 300, and 7000.