Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Masterpact lifting hook and crossbar specification and capacity
Issue: To what standard are the lifting devices designed and what is the weight limit?
Product Line: Circuit Breakers
Environment: Masterpact lifting devices S48900, S48901, S48906

Resolution:
The lifting devices are designed according to ASME B30.20 standards and structural design criteria per ASME BTH-1 design category B, service class 2.

The crossbars S48900 and S48901 have a maximum capacity of 500 pounds.
The lifting hooks S48906 have a maximum capacity of 165 pounds each.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center