This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The D-Frame lube kit is given by the following kit number
625549 KIT, LUBRICATION
The kit contains the lubricant 625550-001 (Castrol EndurexR 4000 lubricant) and the instructions. The lubrication points are confined to the solenoid operator core, core spring, link, shaft, and all other pivot points. Lubricate sparingly.

The lubrication kit can be ordered from the ASCO Parts Department. They can be reached at parts@ascopower.com or at 1.800.800.2726(ASCO) and follow the voice prompt to select the Parts Department.
625549 KIT, LUBRICATION
The kit contains the lubricant 625550-001 (Castrol EndurexR 4000 lubricant) and the instructions. The lubrication points are confined to the solenoid operator core, core spring, link, shaft, and all other pivot points. Lubricate sparingly.
The lubrication kit can be ordered from the ASCO Parts Department. They can be reached at parts@ascopower.com or at 1.800.800.2726(ASCO) and follow the voice prompt to select the Parts Department.
Released for: Schneider Electric Egypt and North East Africa