Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is EVlink Pro AC compatible with the TIC protocol and the French smart meter Linky ?

Article available in these languages: Czech

Yes, by adding the accessory board, reference EVA1MTH / Installation guide GEX2219201.
It is connectable to Historical & Standard TIC and compatible with 3-phase or single-phase
The configuration is done using eSetup,(see below) .



eSetup4