Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can type K cable be used on our ATV212 drive

Issue:
Wants to use type K cable on the ATV212 drive.

Product Line:
ATV212

Environment:
All

Cause:
N/A

Resolution:
Unfortunately, we did not test this kind of cable with our product.
The main issue with the K cable type is the cross section of the cable strand is AWG30. This section is lower than the IEC version we tested in verification and validation test.
Risk is to break some strand when we tighten to the torque specified.

Test in our labs are done with the following cable:

  • Class 5 IEC60228
  • Class C UL486A

So, we can not guarantee the safety with type K cable.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center