Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the purpose of the Transfer Tool that is installed with EcoStruxure Machine Expert Basic?
Issue:
Purpose of the Transfer Tool that is installed with EcoStruxure Machine Expert Basic


Product Line:
EcoStruxure Machine Expert Basic


Resolution:
The Transfer Tool is a console application allowing scripting operations without using EcoStruxure Machine Expert - Basic.
The Transfer Tool allows you to:
  • Download and upload the project to and from the controller.
  • Update the controller firmware.
  • Backup and restore application data.
NOTE: To use the Transfer Tool, you must connect the PC to the controller using a USB cable.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: