Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ZBRT2 does not send signal when slowly released.

The information we give for the ZBRT transmitters, the minimum actuation speed is 0,1m/s and the maximum force is 10N.
Actually, if the operator actuate very slowly the transmitter, it can affect the frames transmitted.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center