Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Can the Series 300 (with the new Group G controller) be used on a different voltage system?
Answer: Yes, a Series 300 (with the new Group G controller) be used on a different voltage system after some changes are made.

HOWEVER, the following parts below MAY need replacing.
  1. Group G controller
  2. Transfer Switch Coil

Furthermore, dipswitch settings and voltage jumper positions must be set properly.

A Group G controller has three (3) part numbers and are rated for certain nominal voltages.
  1. PN 894000-001 – 115V and 120V
  2. PN 894000-002 – 208V, 220V, 230V, 240V, 380V, 400V, 415V, 440V, 460V, and 480V
  3. PN 894000-003 – 277V, 550V, 575V, and 600V

A transfer switch coil is also rated for a certain voltage range. For example, a coil assembly can be rated for 190-240V.

So, if a transfer switch came rated at 3-phase 208V and the customer decided to use it on a 1-phase 240V system, they won’t have to replace any part.  They just need to change some settings (See Dipswitch tables below).

But, if the transfer switch came rated for 3-phase 480V and they need to use it on a 3-phase 208V system, then they need to replace the Group G controller and the transfer switch coil.

Group G Controller Part Number and Jumper Card Position

Group G Controller Phase Configuration Dipswitch Setting

Group G Controller Nominal Voltage Dipswitch Setting

If unsure, contact Technical Support at 1-800-800-ASCO or send an email to technicalsupport@ascopower.com