Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement for the Magelis XBTN400 HMI?
The replacement for the XBTN400 small panel with keypad is the HMISTO715 (4.3" 480x272) HMI.

The HMISTO715 needs a different cut out so adjustments will need to be made. This HMI is programmed using our newest software EcoStruxure Operator Terminal Expert (EOTE), so a new license will be required. The part number for the digital basic license is HMIEELCZLSPAZZ.

It is important to note that it is a different software and the application cannot be converted to EOTE.

Please see the following pages for a comparison of the products:

XBTN400:
https://www.se.com/ww/en/product/XBTN400/small-panel-with-keypad-with-matrix-screen-green-5-v/

HMISTO715:
https://www.se.com/ww/en/product/HMISTO715/touch-panel-screen-harmony-sto-stu-4-3-wide-rs-232-485-rj45/

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: