MODBUS-SL difference with MODBUS RTU
Issue:
The PAS600 documentation refers to MODBUS-SL to describe this communication protocol as available in the product. There is no reference about the specific serial communication protocol named MODBUS RTU.
Product Line:
EcoStruxture Panel Server
Environment:
Industrial communication networks and protocols
Cause:
Technical terminology for communication protocols.
Resolution:
MODBUS-SL (Serial Line) is a way to name the complete serial line protocol, because there is 2 different modes to communicate in serial mode: the RTU mode and the ASCII mode. Each of them, defines the bit contents of message fields transmitted serially on the line and It determines how information is packed into the message fields and decoded.
In summary, when MODBUS-SL is referred as available, you can use either RTU or ASCII communication mode.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.