What can cause an Arithmetic error/Overflow exception with CPU fault code( %SW125=16#DEF2) reported in Unity Pro/EcoStruxure Control Expert?
Issue:
Cause of an Arithmetic error/Overflow exception with CPU fault %SW125=16#DEF2
Product Line:
EcoStruxure Control Expert
Resolution:
If an Arithmetic operation such as a multiplication, addition etc. is performed and the result of the operation exceed the max value for the variable type, this will generate an Arithmetic error/overflow exception. %S18 will turn on and stay on until the cause of the error is cleared. In the example below, IN1 and IN2 when multiplied the result is 40000. This exceed the max value of 32767 for a INT data type and thus the cause of the error.
Cause of an Arithmetic error/Overflow exception with CPU fault %SW125=16#DEF2
Product Line:
EcoStruxure Control Expert
Resolution:
If an Arithmetic operation such as a multiplication, addition etc. is performed and the result of the operation exceed the max value for the variable type, this will generate an Arithmetic error/overflow exception. %S18 will turn on and stay on until the cause of the error is cleared. In the example below, IN1 and IN2 when multiplied the result is 40000. This exceed the max value of 32767 for a INT data type and thus the cause of the error.
Released for: Schneider Electric Egypt and North East Africa
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
Help Center
Find support resources for all your needs, in one place.