Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Does the transfer switch require clearance at the back?
“Front-connected” floor-mounted transfer switches DO NOT require rear clearance.  However, “rear-connected” floor-mounted transfer switches DO.

What does “front-connected” and “rear-connected” mean?

“Front-connected” means that the terminal lugs in the transfer switch are accessible from the front once the door/s are opened.  On the other hand, “rear-connected” means that the terminal lugs are accessible from the rear or back of the transfer enclosure.

See outline drawings below for reference.

Outline - Front and Rear Connect