Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Can I use the “Transfer Test” of the ATS to start the generator without switching load?
No.  The “Transfer Test” feature of the ATS is designed to simulate loss of preferred power and initiate load transfer to the alternate power.  Hence the term “Transfer” Test.

Transfer Test Buttons and Selector Switch