Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How can I prevent / inhibit the Series 7000 Bypass Transfer Switch from switching over to Emergency power?
There are several ways to go about this.
  1. Turn the Emergency power source off (If this cannot be done, please see #2 or #3).
  1. Turn the BYPASS handle to connect the bypass switch to the NORMAL source.
  1. If the Automatic Transfer Switch with Bypass and Isolation switch came with either one of these optional accessories, 30** or 34B, either one can be used to prevent the switch from connecting to the Emergency source.

Acc 30A
Acc 30B
Acc 34

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center