Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Without losing utility power, is there a way to switch to Emergency (generator) power and stay there?
YES.  MOST automatic transfer switches come standard with Feature 17 – “Remote Transfer to Emergency”.

This feature starts the generator and initiates load transfer to Emergency power.  The transfer switch will stay on Emergency power as long as the Emergency Power Source is acceptable and the feature has not been de-activated.  If the Emergency source fails and the Normal source is available and acceptable the switch will return to the normal (preferred) source.

FEATURE 17