Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum voltage per channel for the analog output module BMXAMO0802?

Issue: What is the maximum voltage per channel for the analog output module BMXAMO0802?

Product Line:  Modicon PAC / X80 / BMXAMO0802 / BMXAMO0802H

Resolution: Referring to the Modicon X80 Analog Input/Output Modules User Manual, the output current information is as follows:
BMXAMO0802 Current Output

From the above chart,  the nominal variation range of current and the load impedance of each output channel can be determined, therefore, with this information, the voltage can be calculated given the current and impedance on a DC current loop as shown below:

V=IR

V : DC Voltage in Volts V
I : DC Current in Amps A
R : Impedance in Ohms

V=0.020 A ×350 Ω
V=7 V

In conclusion, the max voltage per output channel is 7 volts; consider that if the device exceeds 350 Ohms, the module may not work as intended.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: