Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the EcoStruxure OPC UA server Expert allow dynamic IP address of the computer without a repair setup for the certificate update?


Issue:
Dynamic IP address for OPC UA Server Expert


Product Line:
EcoStruxure OPC UA Server Expert


Resolution:
Yes, The OPC UA server will support the use of dynamic IP address by way of the /dynamicip command line parameter.. This allows the server to ignore IP address machine modification that would require a setup repair for certificate update. This will help to manage certificates with dynamic IP.  To allow dynamic IP, run the command OPCUAServerExpert.exe /dynamicip.