How can we help you today?

The Logic Editor in RemoteConnect doesn't open

When creating or opening an existing RemoteConnect project the Logic Editor doesn't start.  This can be due to insufficient system memory (RAM).
logic editor do not start
The minimum allowed for the RemoteConnect software version 2.7.3 is 12GB of RAM. 16GB of RAM is recommended.

Schneider Electric Egypt and North East Africa