RemoteConnect error "DTMS not found in the catalog"
After installation, if RemoteConnect is launched and it reports the following error:
This can occur if RemoteConnect DTMs are not installed correctly.
Solution:
- To update the catalogue, try clicking the update catalogue button.
- The installation file for RemoteConnect must be located on the local drive C:.
- Make sure that the downloaded zipped file is unblocked (2-RemoteConnect-R-2.7.3_Ecostruxure-Control-Expert-V-15.1.zip in the screen capture below)
- Verify under the C:\Program Files (x86)\Common Files that the FDT and Schneider Electric Shared are complete.
Released for: Schneider Electric Egypt and North East Africa
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
Help Center
Find support resources for all your needs, in one place.