Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is accessory 31BG?
Accessory 31BG is a Status Relay Bundle that provides a relay (3 total) for each of the following statuses:
  • Normal Source Acceptability
  • Emergency Source Acceptability
  • Pre & Post Transfer Signal
Each relay has 2 NO/NC (Form C) sets of contacts rated for 6A at 120Vac, 250Vac Max.

Please see below for a more detailed accessory description and screen short from a sample wiring diagram.
31BG accessory description

31BG wiring diagram
Please click here for the Group 5 Control Panel User's Guide

For further information you contact Technical Support at 1-800-800-2726 then dial 3 or send an email to technicalsupport@ascopower.com.