Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is accessory 44 strip heater?
Accessory 44 Strip heater is designed to keep the temperature within the ATS enclosure at an acceptable level. This accessory consists of a mounting bracket with strip heater, thermostat and terminal block.

It can be specified in different operating voltages as shown below:
Accessory 44A - 120VAC
Accessory 44G - 208 to 600VAC

Accessory 44A must be connected to power provided by the customer and accessory 44G is powered directly from the load side of the transfer switch.

Please click the link for the installation manual of the Accessory 44 strip heater.

For further information, you may contact Technical Support at 1-800-800-2726 then dial 3 or send an email to technicalsupport@ascopower.com.