Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is feature 17?
Feature 17 is a terminal provision for remote customer contact to perform a transfer to Emergency. When activated the transfer switch will issue an engine start and transfer to emergency until the input is deactivated. If Emergency fails while on Emergency but Normal is still available the switch will transfer back to Normal.
On Group 5 controllers the contact is to be closed to initiate the test. On Group G controllers and all others controllers the input is standardized to be open to initiate the test. Refer to the transfer switch wiring diagram for confirmation of the operation.  This feature is not standard on D frame switches in the 7000 or 4000 Series and instead must be ordered as accessory 17G.

Please see below for a sample Group 5 wiring diagram:

Feature 17 wiring
For further information, you may contact Technical Support at 1-800-800-2726 then dial 3 or send an email to technicalsupport@ascopower.com.