What is the maximum number of ATV320 Drives using the VW3A3616 Ethernet card can be wired in daisy chain?
Issue:
ATV320 Drives using the VW3A3616 Ethernet card what is the maximum you can wire in daisy chain?
Product Line:
ATV320 with optional card VW3A3616 Ethernet card.
Environment:
All
Cause:
Max number of devices can be daisy chained.
Resolution:
Released for: Schneider Electric Egypt and North East Africa
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
Help Center
Find support resources for all your needs, in one place.