Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When converting an M340 project to M580 can you have your IO assigned to Device DDT's in the UMAC tool?

Issue

M340 to M580 conversion with Device DDT's

Product Line

Modicon M340

Modicon M580

Environment

UMAC

EcoStruxure Control Expert

Resolution

Unfortunately the UMAC tool is not there yet. When using State RAM in the M340 the UMAC will put the modules in as topological then create an ST section to move the topological addresses to State RAM addresses. If you used topological addressing in the M340 project, the topological addressing will stay.