Issue
Sage RTU with old firmware is not compatible with newer browsers.
Product Line
Sage 2300, Sage 2400, Sage 3000 Sage 3030.
Environment
Power Metering device, front display.
Resolution
Open Microsoft Edge and enter the IP address for the RTU unit. Then press the Icon for compatibility mode. This is a workaround but it may not work with your current browser version.
A more permanent solution is the Offline Editor or the CPU upgrade. Contact technical support or your sales rep for more information.
Phone: 888-797-6468 (888-PWR-MGMT) Option 7, or
E-mail: sagertu_support@schneider-electric.com
Released for: Schneider Electric Egypt and North East Africa