Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to connect my Control Expert client to the server ?

Before starting Control Expert Topology Manager (TM) on the client side, please follow these steps:

  1. Close TM on the server side.
  2. Open the Server Configuration.
  3. In the Listening Connections tab, update the Listening IP address:
    • Either select the Ethernet card used to communicate with the client PC,
    • Or enter 0.0.0.0 to listen on all Ethernet interfaces.

Server Configuration listenning IP address

4- Apply the changes and close the configuration tool.
5- On the client side, open TM and go to User Preferences.
6- In the Networks and Servers tab, update the Control Expert Server Address with the correct IP and port:
  • For example: IP = 192.168.189.1, Port = 19950.

User Preferences define IP address of TM server

7- Close and relaunch TM on the client side.

You should now be able to connect to the server successfully.