How can we help you today?

P2P Communication Between Simulators in EcoStruxure Process Expert

This Knowledge base article explains the steps on how users can exchange data between the two Simulators with the help of the new implementation of Peer to Peer feature in EcoStruxure Process Expert.
The users should be able to configure the P2P to read variable values from a remote controller or write variable values to a remote controller using the specialized functions of the control participant. EcoStruxure Process Expert’s control participant provides two function blocks ‘READ_REMOTE’ and ‘WRITE_REMOTE’ which can be used to exchange the data between controllers/simulators to read and write information to the remote variables
Note: This feature is available only for the EcoStruxure Process Expert 2021 and above versions
This is applicable for EcoStruxure Process Expert 2021 and above version

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center