Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible two compare two different projects with SVN?

Yes, it is possible to compare two applications with SVN.

In the first step, you must import application A into a repository. For this you must use a SVN tool (TortoiseSVN, VisualSVN) and create a corresponding repository and then you must open the application with Machine Expert and import it into the previously created repository with Project-> Subversion-> Import Project to SVN ...

After importing Application A, you must open Application B with Machine Expert and you have two options how to compare the projects.

Option 1: You can compare Application B directly with a remote project (Project->Subversion->Compare to remote project ...). This function will show you the differences between Application A and B.

Option 2: You can connect Application B directly to an existing SVN project (Project->Subversion->Connect to existing project ...). This function will link Application B to the SVN repository. Afterwards you can see in the device tree all differences between the Application B and head revision (Application A) in the repository. Now you can check the differences between Application A and B step-by-step.