Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What firmware version of the BMECRA31210 is required for the when using the Profibus module PMEPXM0100 in a remote drop?
Issue:
Minimum firmware version of the BMECRA31210 required when using the Profibus module PMEPXM0100 in a remote drop


Product Line:
PMEPXM0100, EcoStruxure Control Expert


Resolution:
BMECRA31210 version V2.40 is required if the Profibus module is used in a remote drop.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: