Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why do I get the error message "Vijeo-Designer Lite version 1.3 must be installed" when installing SP1 and I already have Vijeo Designer Lite V1.3 installed?

Issue:
Error message during the installation of SP1 for Vijeo Designer Lite V1.3


Product Line:
Vijeo Designer Lite


Resolution:
The error message below is generated when Vijeo Designer Lite is installed on a non-supported operating system such as windows 7/10/11 64 bit. Vijeo Designer Lite is supported on Windows XP/ Windows 7 32 bit only.

image1

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: