How can we help you today?

How can you set up an ATS480 Soft Starter with an AB Compactlogix PLC?

Issue:

ATS480 Soft Starter with an AB CompactLogix PLC?

Product Line:

ATS480

Environment:

All

Cause:

Serial communications between ATS480 and AB PLC.

Resolution:

ATS480 Ethernet/IP Integration with Allen Bradley CompactLogix PLC

Refer to all ATS480 documents for the proper installation procedure.

User Manual NN8Z85515

ATS480 Ethernet IP manual

User manual NNZ85540

AB PLC FAQ 1

Insert a VW3A3720 EIP/Mdb TCP Dual port communication card into the module slot.

Ensure the VW3A3720 card is updated to the correct firmware for use in the ATS480.

VW3A3720 Compatibility ATS480 soft starters with, at least, V1.1IE01 software version, are only compatible with VW3A3720 Ethernet module versions V2.1 and higher.

Consult with the Drives Product Support Group for Firmware procedures, Firmware, DTM’s and keypad LANGUAGE file.

Ensure control power is properly connected to CL1 and CL2:
d
It is also required to have 24VDC present on the STOP terminal to enable network start/stop.  If this voltage is missing, the ATS480 will remain in nSt state and unable to run.
A hardwired E-Stop or shutdown circuit can be wired between +24 and STOP so that the circuit is closed when allowed to start and is open to stop.  If no external interlock is needed a jumper can be installed between +24 and STOP, but be sure to evaluate the safety of this for your specific installation.  See manuals for details.

AB PLC FAQ 3

AB PLC FAQ 5

AB PLC FAQ 6

AB PLC FAQ 7

d

AB PLC FAQ 9

AB PLC FAQ 10

AB PLC FAQ 10

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center