Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you change or add a new username with the cyber security feature on the ATS480 Soft Starter?

Issue:

Changing or adding a new username when connecting with Ethernet on the ATS480 Soft Starter

Product Line:

ATS480 Soft Starter

Environment:

All

Cause:

Cyber Security feature

Resolution:

No, you cannot currently add a new username or change the username from ADMIN. You can only change the password or deactivate the cyber security feature.