Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the QO260GFI3W be used for 240Vac application?

Product Line:
QO Branch Breakers

Resolution:
Yes, the QO260GFI3W will work the same as QO260GFI for circuits without a load neutral. Connect the two hots to the two hot screws, connect the neutral pigtail to the neutral bar, and leave the load neutral screw empty.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: